Hello all,
I'm working with TI PLC Development Kit ( AFE031+ F28069 ). Can I use the protocol PRIME for the communication between PLC modems when one is connected to the primary winding and the other one to each of the two secondary winding of the transformer at a distance of 5m on each side, or I must use the protocol G3 for this communication?
Thank to all,
Roberto