We are testing an F28335 chip on a custom board and have access to the JTAG interface. We have specific (static?) memory addresses that we would like to PEEK/POKE while the program runs (though understandably we'll have to halt the chip) but as we aren't the party who built/programmed the board, we don't have access to the source nor can we reprogram the chip, say, in debug mode. Note that I believe the program is custom as well and does not use any DSP/BIOS or RTA/RTDX libraries.
Is it possible to perform these simplistic memory PEEK/POKE operations on such a setup? I have an impression that in order to do the standard CCS "Memory Browser" type operations we need to have the source and build it in Debug mode, then program, though hopefully that isn't the case. We are a little familiar with DSS, so using this is possible as we may want to automate these tests going forward.
To restate the question (hopefully more simply), is it possible to do simple memory read/writes to specific addresses via the JTAG interface on a chip that is already programmed and cannot be reprogrammed?
Thanks!