Hi all,
I am writing a new project with dual core in TMS320F28377D.
configuration mode is Debug.
No error is coming while of both the core is built.
But while I run the project(dual core) it seems that CPU1 is responding while CPU2 is not.
I am using the include, linker files and source files from controlsuite with V130.
However same problem is not coming with same softawre ( main.c) while the include. linker and source files are taken from V110 or V120.
Have anyone faced this problem. Please help.
Regards
Raja Saha