I have a new F28377D card, and am trying to get the example project "usb_dev_serial" from ControlSuite running as a start point for something. The comments in the code state:
//! Connect USB cables from your PC to both the mini and microUSB connectors on
//! the controlCARD.Figure out what COM ports your controlCARD is enumerating
//! (typically done using Device Manager in Windows) and open a serial terminal
//! to each of with the settings 115200 Baud 8-N-1. Characters typed in one
//! terminal should be echoed in the other and vice versa.
The FTDI virtual COM port through the mini USB connector is fine and shows in device manager as 'USB Serial Port (COM4)', but when I compile and load the program, the other COM port (the one through the micro USB, direct to the chip) is not recognised by my PC. It shows up in device manager, but just as 'Virtual COM Port' with a yellow exclamation mark and no driver. In this state, I cannot communicate with it via a terminal window.
Is there any driver available for this, or anything else I need to do to be able to get this running properly?