Hello I am trying to do lab 2 of this workshop http://processors.wiki.ti.com/index.php/C2000_SolarWorkshop
But I am having a hard time with lab 2 where on step 20 of the lab 2 PDF which can be found in SolarWorkshop_Software/SolarWorkshop/workshops/SolarWorkshop/~Docs
On the lab 2 pdf on part 25 where it asks to change the value of MPPT to 1. Doing this drops my Vref value and MPPT actually does not kick in to adjust the Vref to work. As far as my hardware goes I have all the main jumpers populated. I do not have M7 J4 populated as it was directed that this is only for GUI control.
Can someone help me? Also this kit only came with 5 jumper connections, is this normal?