I just recently uninstalled both controlsuite and CCS. Then downloaded and installed controlsuite and checked for updates, that went fine with no errors. Then downloaded and installed CCS and checked for updates. This is where the first problem occurred. You can see below the errors I received when trying to update CCS.I then continued to try and load M3, that went smoothly but then when I moved on to loading the C28 I received the errors shown in problem 2. This is being done using a TI example program.
(1) Problem during installing updates:
‘Computing size’ has encountered a problem.
An internal error occurred during: ‘Computing size’.
Detail:
An internal error occurred during: ‘Computing size’.
Profile epp.package.cpp is marked as changed.
(2) Problem with loading C28 project (for SW1: up, down,down,down and SW1:up, up, down, down)
C:\ti\controlSUITE\device_support\f28m35x\v205\F28M35x_examples_Control\blinky\c28\ccs\Flash\blinky_c28.out: a data verification error occurred, file load failed.
The message in “Console”
C28xx_0: GEL Output:
Memory Map Initialization Complete
C28xx_0: GEL Output:
RAM Initialization Complete
C28xx_0: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
C28xx_0: File Loader: Verification failed: Values at address 0x000000000013E6D4 do not match Please verify target memory and memory map.
C28xx_0: GEL: File: C:\ti\controlSUITE\device_support\f28m35x\v205\F28M35x_examples_Control\blinky\c28\ccs\Flash\blinky_c28.out: a data verification error occurred, file load failed.
I hope you can find the time to help me out, and thanks for all the help.
Joshua