DEAR
I begin to use CCS6 recently.There are many problems confuse me.
1 CCS6 often display “NO RESPONE” then HALT.
2 After close the CCS6 , the CCS6 don’t release the WORKSPACE.
You must reset PC before another CCS6 running.
3 In the EDIT MODE , The HALT fault have low freqency.
But There are high freqency in the DEBUG MODE
4 I use PC and NB to try it, The results are identical,
PC is WIN-XP pro SP3 +CPU INTEL G630(2.7GHZ) RAM 2G
NB is WIN-7 home SP1+CPU is INTEL B940(2GHZ) RAM4G
5 The test code is very simple.
int i;
for(;;){
i++;
}
6 I use LAUNCHPAD F28027F as target board.
Do anyone can give some suggestions?