Hi all,
I have made a customized board using the TMS320F28335 processors. The problem which I am facing is quite strange. Before going to the issue let me take a minute in explaining the my boards configuration. The board has got two external devices connected on the external bus( XINTF) an A/D convertor & a Ext UART.
I have configured my ckt so that only one device remains active on the bus either the A/D or the UART.
Now coming to the issue.
On the A/D converter I perform a 16 bit read operation only which is working fine.
But when I perform a Write operation on the UART I don't see any activity on the data lines whereas the address and other control line behave normal. To take away the effect of my external circuitry I have even isolated my ckt with the DSP and tried to write on the external bus but the problem persists. NO ACTIVITY ON THE DATA BUS. can anybody explain so as to why this is happening?????
Regards
SHIJESH