Hi,
The Hi-res deadband rising edge control doesn't work correctly. Here's how I ran into the issue:
1. Enable MEP deadband control for both edge: EPwm1Regs.HRCNFG2.bit.EDGMODEDB = 0x3;
2. Set normal Deadband rising edge to 2 or 3: EPwm1Regs.DBRED = 2 (or 3)
3. Try changing EPwm1Regs.DBREDHR.bit.DBREDHR => the deadband doesn't change as expected.
The MEP deadband control works well with DBRED NOT equal to 2 or 3 and well for falling edge.
Bug is when rising edge with Normal deadband set to 2 or 3.
Is that a bug with the new chip?