When I debug the USB of F28377D, I can read out the file and data from the U-disk,but can't write to the U-disk.
FYI:
1) Engineering Sample Chip version:
|TMX320F28377DPTP |
| YFB-46AQ3HW |
| G4 |
2) controlSUITE version 3.3.0
The error msg:
USB debug loop in the function USBHCDPipeWrite( ) and can't receive the flag of ePipeStalled
else if(g_sUSBHCD.psUSBOUTPipes[ui32PipeIdx].iState ==
ePipeStalled)
I doubt about this problem only happen on the Engineering Sample Chip or the example code?
any TI Employee can confirm this problem?