Hello,
I am using CCS v 5.5.0.00077 and motorware_1_01_00_13. Should I upgrade to the new free version of CCS 6? I have a paid for license 5.5. I will have a paid-for license CCS 6 in a few weeks. I was wondering what kind of conflicts I might run into by downloading and installing the free version of CCS 6. Should I remove CCS 5.5. or does CCS update it even if it is the free version?. Or do both the programs run on the same hard drive without any conflicts. Same with motorware 13 v 14?
Chuck