Hello,
Working with sdk TMDSPLCKIT-V3 I'm trying to send big prime packets using PLC modem. I've done a program that increments the size one byte and send it to a meter.
The problem is that when it reachs 371 bytes in the payload packet (total size: 371+9 bytes generic and mac header+4 crc bytes)) it can't send nothing bigger and stops to send anything else.
The question is, are there any limit or bug in the PLC modem to send big packets (500-600 bytes)?
Thanks in advance,
Rubens