Hello,
I currently have a 28069 control card that I have wired up a eeprom to via I2C. I am using CC5 version 5.5.0.00077.
I can run the example and it passes (i.e. it writes 2 bytes and reads 2 bytes successfully from the eeprom).
When I change the number of bytes to anything larger than 2 (via the I2C_NUMBYTES #define at the top of the file) it does not complete the transactions and the reported status is I2C_MSGSTAT_WRITE_BUSY.
Any idea what I could be doing wrong?
Thanks,
Brent