What is the maximum frequency that data can be transmitted via the USB (JTAG XDS100V2) connection? I need to perform some measurements on the encoder of my motor, and I want to extract the rotor position (500 counts/rev) as accurately as possible, while the motor performs a given speed trajectory (about 1000 rpm).
If the USB connection is not suitable, what is an alternative?