Thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In CCS memory watch window, can you check the value in different flash sectors ? If you see all the values as 0x0 then device is LOCKED (which could be because security PASSWORD location got programed with value 0x0) and there is no way to recover the device in such case.
You need to replace the device on the board.
Regards,
Vivek Singh
Samir,
Earlier you were not able to program the code into RAM as well. What change you made to get it working? If password location are all 0xF then you should not have any issue with Flash loading. Can you try erasing the Flash sectors using CCS Flash plug-in (GUI) and see if that works. Also if you have another board, please see if that works fine.
Regards,
Vivek Singh