i tried to run the sci echoback example and i can receive from the processor i can see the first messages on hyper-terminal but when i tired to send data to f28069 i cant receive it. i figured maybe there is a problem with hardware setup because i went through the codes and i cant see any problem. is there anything hardware configuration i have to do on the board before using SCI with f28069? anything i have to change??
thanks