Hi, Everyone
I need your help.
I watched this thred.
Devin Cottier says "The following sequence may be necessary to unlock 16-bit mode"
*Connect to the device
*Perform a debugger reset in CCS
*Set a hardware breakpoint at the reset vector in the dissasembly (current location of the PC)
*Load the symbols for the test program to CPU1
*Manually reset the device via XRSn
*View DevCfgRegs.PERCNF1.all in expressions window (may require refresh if already in window)
*Write 0x0000 to above register
*Hit run twice in CCS, should end at "ESTOP0"
*Load test code
*Run test code
*Further code can be loaded and run without issue until power cyle/XRSn reset
It seems to see same things on ADC Errata : Analog Trim of Some TMX Devices.
Actually is this operation required except workaround of Errata ??
Best Regards
Hiroyasu