Hi,
I want to generate PWM using and TMS320F28335 and Code Composer Studio (v 6.1.0) and analyse the same using oscilloscope.
Can someone please help me on this.
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to generate PWM using and TMS320F28335 and Code Composer Studio (v 6.1.0) and analyse the same using oscilloscope.
Can someone please help me on this.
Thanks!
Hi,
I would recommend that you download and install controlSUITE which provides most of C2000's code examples and kit collateral.
Once installed, I'd recommend looking in the following directory for an ePWM example:
\controlSUITE\device_support\f2833x\
Hopefully this helps!
Thank you,
Brett
Hi Gautam!
Thank you for the reply!
I imported the project and was able to build the same.
Could you please let me know the procedure on how to dump this build on TMS320F28335F using JTAG emulator.
Vinay
Could you please let me know how to check XRS pin status and boot pin status? Voltage level is 5V.
XRSn should be pulled high with 2.2k resistor, TRSTn is pulled low with 3k resistor.
Boot Pin:
I hope you know that F28335 functions at 3.3V and not 5V logic and hence a 3.3V regulator should be present after 5V.
Regards,
Gautam
Laxmi Narasima Vinay Gattu said:With the 3.3V logic and pull up and pull down resistors, that error is resolved. Thank you!
Excellent! (Please verify the answers whenever you find one. This helps a lot for other community members.)
Laxmi Narasima Vinay Gattu said:When do we get to know that the program is loaded on the hardware? Because when I click on debug it is showing as "running" and stays here for so much time. Will there be any message showing that the build is loaded on the device?
The Green Play symbol would be highlighted when the loading is done. All you've to do is press this button for the program execution.
Regards,
Gautam