I'm using 28346 external interface XINTF with following configuration:
USEREADY=0, X2TIMING=0, LR=3, AR=7, TR=0, LW=3, AW=4, TW=3
In this configuration LR, AR, LW and TW are at the maximum and can't be increased anymore.
To increase the wait states I need to set X2TIMING = 1.
The restrictions for X2TIMING=0, USEREADY=0 are:
LR>=2, AR>=6, TR>=0, LW>=3, AW>=1, TW>=3
The Data Sheet says: "If X2TIMING is enabled, specified Lead, Acitve, and Trail restrictions can be divided by 2 for values with even numbers."
An appropriate configuration (from my external IC point of view) would be:
X2TIMING=1, LR=2, AR=4, TR=0, LW=2, AW=2, TW=2
Is this a valid configuration?
Thanks for an clarification.
Uwe Grossmann