Hi all,
I am doing some work with the lab examples and have run into a little problem whilst following some of the calculations in the pdf.
The KpSeries value has to be calculated using the controller Bandwidth as shown below.
In order to get the controller Bandwidth value I have to make the following calculations.
In this formula the sample frequency (Fs) needs to be filled in, however there is no explanation on how to get this value.
The example right above this formula shows a sample frequency of 10KHz. But is this specific to the motor they are using in this example or is this a general value that can be used with any motor?
Thanks in advance,
Michiel Vanrompay