Hello,
I use the TMDSHVMTRPFCKIT with the F28335 control board.
My IDE is CCS v3.3, and I use automatic code generation with Matlab/Simulink. I use the onboard USB-JTAG debugger.
When I generate the code, compile and download the code in RAM, all works fine.
When I download the code in FLASH, the DSP does not restart automatically when I restart the DSP power (code generation and download is OK because I use the same on another application and that works fine). I think my problem comes from the jumpers configuration on the PCB : I tried different one but didn't find the one that works. I don't think I have to modify the jumpers on the DSP controlboard itself because on another application I didn't modify them and it runs correctly at restart.
I remarked that after having flashed the DSP, when I restart the power, simply connect CCS then clik on "run", the DSP starts correctly.
Do you know how I have to configure the jumpers on the kit's PCB for the DSP to start automatically from FLASH ?
Shall I add any pull-up/pull-down on the JTAG side to force the DSP to start?
Thank you,
Best regards,
Julien