I am going through the IDDK Development kit user guide procedure and everything works great the first time but after that the expression variables in figure 10 of the user guide are set to zero except the enable flag which continues to be set to 1.
I followed step 18. to Reset the target on program load or restart. Then step 19 says to disable the silicon real-time mode button before resetting the CPU. This I have done.
I stop the program according to the instructions in the user guide. The second time I go through the steps when I click debug the program automatically starts running without ever hitting the run button. The variables in the expression window still remain from the previous debug however their values are now all set to zero!
How can I prevent the values in the expression window (and thus the .c file) from being set to zero when I reload the program a second time?
Thanks,
Adam