Hello ,
I am working on controlling the jitter between the cpu clock and the ADC clock , during acquisition sequences.
For instance, i am performing a full sequence acquisition using the sequential mode based on 8 input channels, using SEQ1 sequencer.
Knowing the following steps :
1- configure the auto conversion mode to OFF
2- reset the sequencer ,
3- trigger the SOC
4- Wait that the SEQ_CNTR reaches 0 (through a loop and ADC status word)
5- TOGGLE GPIO5
I expect to have the same number of CPU clocks between steps 4 and 5 each time this full sequence is performed.
I expect no jitter between strep4 and 5 But i still have a jitter of 1 CPU cycle
Did any one face this issue to provide synchronization with the ADC clock ?
Thank you