Hi all,
I am using F28069 to send multiple bytes data in one transmission via I2C.
Here is what I want:
Send START condition, SLAVE address, EEPROM address High, EEPROM address low, 64 bytes, STOP condition.
When I look at the reference guide. It shows the I2C's FIFO is only 4*16 bit size. How can I send 64 bytes data before the I2C module generates a STOP condition.
Thanks
Fei