I have a TMS320F28069PZ which is supposed to control three BLDC motors through motor drivers, using PWM.
I have made a program which turns on an onboard LED as the first thing in the main()-loop. This works perfectly when I click the debug-icon in CCS.
However, if I disconnect the JTAG, and then turns the MCU-power OFF and ON, the program does not seem to start, because the LED does not turn on.
Is there any special steps I need to take to:
A) Transfer the code to the MCU's onboard memory
or
B) Make the program start automatically when the MCU is powered on?
Thank you in advance