Hello!
I am trying to load my first program to TMS320F28054M. It is a custom board and hence the chip is empty, so I am trying to burn my code to it using SCI bootloader with the help of Flash Kernel. I already implemented this many times on 28027 chip and everything worked perfectly.
I do start the flash Kernel through the Visual Studio (verbose option enabled). It burns the Kernel, then starts application update, does auto baudlock, and then exits the application. The thing that looks suspicious to me is that the Controlsuite contains only example for 28055 chip (f28055_flash_kernel), I wonder if it is compatible with 28054M? Both devices have the same flash memory map (at least according to this document), but maybe I'm still missing something.
Thanks in advance.