So I'm trying to compile the BlinkLED from basic example codes, and the code does compile, but when I try to upload it, this is the message I get.
Ensure a jumper is placed on JP7 and that the jumper is removed from JP6, and that the boost switches (S1) are ON-OFF-OFF (UP-DOWN-DOWN), and press the reset button before clicking OK. If the download fails try a baud rate below 38400.
And the problem is, I'm following the instruction perfectly except for the baud rate for that I don't know how to adjust it. But I already set board and serial port configuration same as the video that Texas Instruments uploaded on Youtube. So I'm wondering if anyone could come up with an answer and help me with this.