HI
i am using delfino377d controller in that GPIO20 is not working.with same configuration other GPIO like GPIO19 working properly.
TOGGLING of GPIO19 comes properly but GPIO20 not coming with evalution board also i tried. please give me solution.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI
i am using delfino377d controller in that GPIO20 is not working.with same configuration other GPIO like GPIO19 working properly.
TOGGLING of GPIO19 comes properly but GPIO20 not coming with evalution board also i tried. please give me solution.
yes i intialized properly i tried with example code.same configuration GPIO 19 working properly
i am using => control suite v3.3.0
path => controlsuite/devicesapport/F2837xD/V150/ExamplesSPU1/gpio-toggle
Hi Raghu,
Did you check the respective bit in GPIO DATA register in CCS watch window to confirm the value expected on output is atleast reflecting in this register?
Also it'll be good if you could post the non-working code here.
Regards,
Vivek Singh
the below code i used in application.this is also taken from example.with these functions other GPIOS working fine
GPIO_SetupMUX(20,GPIO_MUX_CPU1,0);
GPIO_Setuppinoptions(20,GPIO_OUTPUT,GPIO_PUSHPULL);