This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GPIO Mux Values, I2C Problems SCL and SDA Pins

Good Morning


Im using a C28027 in simulink with the library "embedded coder" and i have problems to enable the I2c Pins SDA and SCL. First, can i enable what pin i can use to I2C??

when i compilate a program using I2c blocks in simulink and compilate with the Ccs 3.3 all the possible I2C pins stay in high value (3.3 volts), i mean that i cant see the clock signal in the SCL pin


i read something about a "mux values" how can i configure or change the "mux value"?


in the peripherals of the target only show me that in the i2c section

but in another targets show that, and can i assigned the pins

PD: i dont understand the example of I2c comunication for a EEPROM in that library

im trying to read a MPU6050 using simulink with I2C but first i need check the I2c comunication, that i say "i cant see the clock signal in the SCL pin"