I want to generate A sin(Wt) with A and W as external signals. As shown in figure i have done that. Sample time for blocks is 50e-6. I am using this block in inverter control algorithm. After downloading code on F28335 controller, it stops controlling after 5 min 30 sec. p.s. if i use inbuilt sine source block, it works fine. But, i want A and W configurable from external signals.
in.mathworks.com/.../238181-control-algorithm-stops-working-after-5-min-30-sec-on-f28335