Hello
I am developing TMS320F28335 interface to a slave with async serial communication at 2.5Mbps
While the upper limit of SCI is 4.67Mbps, I am having problem to match it to 2.5Mbps
With LSPCLK set to 75Mhz
I noticed that I can configure SCI to either 3.13Mbs or 2.34Mbps but not 2.5Mbps. 2.34Mbps give me ~6.4% of error which is over 2% the recommended limit.
Slowing LSPCLK does not bring me closer to 2.5Mbps as well.
Any thoughts on getting the SCI closer to 2.5Mpbs
Alan