Hi,
I wish using the XCLKIN in TMS320F28027. I use the following code:
myClk = CLK_init((void *)CLK_BASE_ADDR, sizeof(CLK_Obj)); myCpu = CPU_init((void *)NULL, sizeof(CPU_Obj)); myFlash = FLASH_init((void *)FLASH_BASE_ADDR, sizeof(FLASH_Obj)); myGpio = GPIO_init((void *)GPIO_BASE_ADDR, sizeof(GPIO_Obj)); myPie = PIE_init((void *)PIE_BASE_ADDR, sizeof(PIE_Obj)); myPll = PLL_init((void *)PLL_BASE_ADDR, sizeof(PLL_Obj)); myWDog = WDOG_init((void *)WDOG_BASE_ADDR, sizeof(WDOG_Obj)); WDOG_disable(myWDog); CLK_enableAdcClock(myClk); (*Device_cal)(); CLK_disableAdcClock(myClk); CLK_setOscSrc(myClk, CLK_OscSrc_External);
The problem is that in gpio.h do not have the "GPIO_setMode" suitable for XCLKIN (GPIO_19 because I'm using the board Piccolo). I have not found in ControlSuite code examples using the XCLKIN. I appreciate any help.
.,
Danilo.