Hi there,
I have some problems with the cmd file for a Buck_VMC_F28069M project,the code is in F28069_FLASH_DP_BoosterPack.CMD file,line 57-61
FPUTABLES : origin = 0x3fd590, length = 0x0006A0 /* FPU Tables in Boot ROM */
IQTABLES : origin = 0x3fdc30, length = 0x000B50 /* IQ Math Tables in Boot ROM */
IQTABLES2 : origin = 0x3fe780, length = 0x00008C /* IQ Math Tables in Boot ROM */
IQTABLES3 : origin = 0x3fe80c, length = 0x0000AA /* IQ Math Tables in Boot ROM */
IQMATH : origin = 0x3fe8b6, length = 0x000afa /* IQ Math functions in Boot ROM */
but as the Memory Map of On-Chip ROM Figure given in technical reference guide,why is it not configured as below:
FPUTABLES : origin = 0x3fd860, length = 0x0006A0
IQTABLES : origin = 0x3fdf00, length = 0x000B50
IQTABLES2 : origin = 0x3fea50, length = 0x00008C
IQTABLES3 : origin = 0x3feadc, length = 0x0000AA
IQMATH : origin = 0x3feb86, length = 0x000afa
what's more,the start and end address of IQ Math Functions are 0x3FEB86 and 0x3FF3B0,0x3FF3B0-0x3FEB86=0x82A,I don't know why the allocated table size for IQMATH is 0x000afa instead of 0x00082A