Hi,
Flash API documents for previous C2000 microcontroller generations (e.g. "TMS320F2833x Flash API", Version 2.10) tell that the erase function disables interrupts for 3 - 4ms and the callback function is invoked every 3 - 4 ms.
In the Flash API document for the F2837xD Flash API (Literature Number SPNU595) I did not find sections on callbacks or disabled interrupts. So my questions on the F2837xD flash API functions are:
What are their worst case execution times?
Can they be interrupted?
Do they support callbacks? - if yes: What is the maximum time between callback invokes?
Thanks, Dieter