In analog control circuits, I've always calculated the low frequency gain of the modulator in a buck topology as the input voltage divided by the peak of the sawtooth. For a boost I think the low frequency gain is the output voltage divided by the peak of the sawtooth (which I think is more of an approximation).
Since a PFC circuit is a boost topology with an inherent inner current loop and with a changing input voltage, how do you determine the low frequency gain of the modulator? How can you properly compensate the outer voltage loop of you do not know the low frequency gain?
Also, I'm performing digital control of power supplies with a TMS320F28335. If I want to control a buck converter, and I use the input voltage divided by the peak of the sawtooth to determine the low frequency gain, what amplitude do I use for the sawtooth? I assume it is 1 volt, but this gives me a tremendous amount of gain for the 350 VDC power supply that I'm controlling.