Hi,
I am using a F28M36 controlCard Experimenters kit in which i got a doubt regarding the Ethernet section.In this section it is specified that the Ethernet controller used is "TLK110PT". According to the data sheet of this part,it is given that the pins PFBIN1,PFBIN2 for core supply should not be given a voltage greater than 1.8V.But in the schematics provided for the kit,3.3V is given to these pins.I've checked this and got 3.3V at these pins.Please clarify this.
I am attaching the part TLK110PT data sheet.Note that I've not tested the Ethernet functionality yet.
Thanks in advance,
Naveen,tlk110.pdf