Any one can help is really appreciated.
I am trying to use TMS320F28335 device(of default system clock 150MHz) with 20MHz external oscillator. It displays the following error.
C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: GEL: File: C:\Users\user7\Desktop\VI_Sensor_Matcher\Matcher_New_program\Debug\Matcher_New_program.out: Load failed.
Is the external Oscillator necessarily be 30MHz ? Can I configure the device to 100MHz with 20 MHz external Oscillator ?
Thank you very much