I have two HVPSFB units. I can run them independently in regular PCMC mode and in constant current(CC) mode. However, when I connect their output together to the same load, the CC unit will no longer supply constant current output. It seems like the presence of the correct output voltage as generated by the unit in PCMC non-CC mode confounds the unit in constant current mode. Any ideas? Thanks!!!