Hi!
I'm using the control card of F28377D Delfino Experimenter Kit. I designed my own docking station for the card.
I met a problem with ADC module.
I used two resisters working as a voltage divider for the AD input of the control card. The designed amplifying ratio is 0.66. The docking station works well without the control card. The ratio stays at 0.66. However, after the control card is installed onto my docking board, some of the ADC inputs's ratios turn into 0.63 no matter how many volts are applied.
I use ADCA0-5, ADCB0-5 and ADCC2-5. The change of the amplifying ratio only happened on ADCA0, ADCA1 and ADCB1. The others work well.
I'm confused and I wonder why.