Dear TI professionals,
I am working with DRV8301-HC-EVM kit and brushless motor Turnigy GliderDrive SK3 Competition Series - 3858 - 4.6 840kv.
When adjusting DfuncStartup and CmtnPeriodTarget, I cannot get the motor to stop vibrating while spinning.
As stated in the guide: "The parameters DfuncStartup and CmtnPeriodTarget should be such that, at the end of motor speed up phase, the generated Bemf is lower than the average voltage applied to motor winding. This will prevent the motor from stalling or vibrating."
Some motor parameters:
RPM/V: 840kv
Motor Poles: 14
Internal resistance: 0.031 Ohm
Max Loading: 45A
Max Power: 830W
Any help would be greatly appreciated.