Hi,
I am currently using Motor control + PFC dev kit TMDSHVMTRPFCKIT (TMS320F28035 control card).
I am using the code from following directiory C:\ti\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v2.1\HVACI_Sensorless_PFC_F2803x
After debugging the above code PFC block gives the 300 VDC which is not sufficient to driver the motor (as per TI documents) In this code i changes only the BASE_VOLTAGE 220,BASE_CURRENT 1 and BASE_FREQ 48 .
Input source is 220 volt AC
As per the documents at the output of PFC block min 350 VDC require .
please anyone tell me what should i do to get the required voltage.
Thanks in advance...............