My application runs on a TMS320F2812, it runs from FLASH and uses IQmath. I'm using the linker command provided by TI (F2812). I'm using CCS 6.
The user manual for IQMath makes reference to a section IQmathTablesRam that is allocated to RAM and PAGE = 1 (data). F2812.cmd does not make any reference to this section. Only IQmath and IQmathTables.
The questions are: Do I need to add IQmathTablesRam to my linker command?
If the answer to the previous question is affirmative... Can I allocate the section to flash? e.g.
IQmathTablesRam : > FLASHD PAGE = 1
Why is it that in some examples this section uses PAGE = 1 and in some examples this section uses PAGE = 0 ... if it is a data section ...
shouldn't it be PAGE = 1?