I have questions for ADCoffsetSelfCal function
1. TMS320F28027 dosent have "B5". SO how it will conect VREFLO to B5.
2. The settings are not normalized after the function returns to normal
for example // ADCINT1 and ADCINT2 is disabled at the end of the function. However, the settings
1.// Disable continuous sampling for ADCINT1 and ADCINT2
2./ADCINTs trigger at end of conversion
3.// Setup ADCINT1 and ADCINT2 trigger source
4. // Setup each SOC's ADCINT trigger source
are not disabled at the end of function or u can say to there default value.
3. Will it affect my ADC samplig which are programmed to trigger by CPU timer. As in above said function they are triggered from ADC interrupts and are force start.
4. As my running above function periodically to reduce offset error, will it affect my existing ADC settings or I have to make my ADC settings again