Hi,
I am trying to work with the TMDSPLCKITV4-ARIB kit. I am interested in LMAC mode in the first phase. As I understand, this mode allows me to transmit and receive packets without any routing protocols, am I right?
I have configured the module to LMAC mode, but I cannot understand from the TI_G3_host_msg user guide how do I use this mode. The DATA_TRANSFER message type (00) allows sending packet in LMAC mode, but it requires "HCT Connection Handle". Where do I get this handle? It says that this handle is generated by CONNECT command, but I cannot see such command in the user guide....
Any help appreciated...
Alexey.