I am trying to write the Park transformation with using _IQsin function from IQmath for motor control with PWM.
I have the TMS320F28335 processor with board eZdsp F2812 and example Example_2833xEPwm3UpAQ.c
And when I add the _IQsin command in my programm I have the error:
Available memory ranges: IQTABLES size: 0xb50 unused: 0xb50 max hole: 0xb50 IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD warning: entry-point symbol other than "_c_int00" specified: "code_start" error: errors encountered during linking; "Example_2833xEPwmUpAQ.out" not built
As far as i understand i should to change the file 28335_RAM_lnk.cmd.
But unfortunatelly I am a not good specialist in programmig. Please help me, what should i write to 28335_RAM_lnk.cmd file that the IQTABLES have enough space for calculate _IQsin and _IQcos functions?
I am also trying to use 28335_IQmath_lnk.cmd but I have the same problem.