Hi,
We are using RS232 interface for Serial Flash programming using SCIA boot mode, and working properly for TMS320F28335.
Can I use RS485 (Half-Duplex) interface for the same?
Regards,
Bhavin Joshi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are using RS232 interface for Serial Flash programming using SCIA boot mode, and working properly for TMS320F28335.
Can I use RS485 (Half-Duplex) interface for the same?
Regards,
Bhavin Joshi
Hi Gautam,
Look at my setup for serial boot loading in TMS320F28069
GPIO29(TX) ---> (pin 4) SN65HVD12D
GPIO28(RX) ---> (pin 1) SN65HVD12D
GPIO19(DE/RE) ---> (pin 2&3) DE/RE of SN65HVD12D
I've tried with RS485 to RS232 converter, but failed to communicate.
Device communication failed in Auto baud.
Any suggestion for this?
Regards,
Bhavin Joshi