Hi,
Processor is an F28335.
Getting this error when trying to download code:
C28xx: Error connecting to the target: (Error -1015 @ 0x0) Device is not responding to the request. Device may be locked, or the debug probe connection may be unreliable. Unlock the device if possible (e.g. use wait in reset mode, and power-cycle the board). If error persists, confirm configuration and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.641.0)
Started to get this error message this afternoon. What does it mean? I can't find any documentation for it. I suspect the device may well be permanently locked... Is there anyway of finding out?
The connectivity from the JTAG is fine, the issue seems to be a Locked Device...
I've seen the Uniflash tool and wondered if I can unlock using this? The problem is I have never set a password and wouldn't know what it is - unless there is a default?