Hello Folks,
We are facing one problem with SMJ320F2812. The device wired in one card cannot be flashed. It is showing following error when we try to Flash it.
"C28xx: Flash Programmer: Error erasing flash memory. Device is locked or not connected. Operation cancelled
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
C28xx: Trouble Writing Memory Block at 0x3f7ff6 on Page 0 of Length 0x2
C28xx: GEL: File: C:\Documents and Settings\xxxx.out: Load failed."
We have wired and tested many SMJ320F2812 in the past using the same circuit and first time facing the problem. While we monitor the Reset pin, it is showing a pulse of 32us width low at a periodicity of 125 Hz. Our clock freq is 80 MHz. The device is powered from TPS70358 and TPS7A4501.
Please help us with the solution.
Thanks,
Srijan