Hi,
I have some questions about HVPSFB-PCMC's HVPSFB-DPL-ISR.asm(TMS320F28035). These problems have troubled me for a lot of days.
1) The interrupt setting is "EPwm1Regs.ETSEL.bit.INTSEL = ET_CTRU_CMPA". So I think the interrupt frequency is 100KHz, but the user's guide(TIDU248) say "a run-time section which executes at twice the PWM". How? Where is it setting?
2) To implement the SR's dead band because of "EPwm4Regs.DCFWINDOW" or those NOPs?
3) Dmax=0.734375 and the HVPSFB-DPL-ISR.asm is around 165 cycles max, could these two things be related?
Thanks!