I am trying to send the data to the DSP from PC through UART Communciation, When I am running the code from RAM, it is sucessfully working, but when I am running the code from the Flash it is not working. Even though I am running the code from flash during boot process I am copying entire Memory sections into the RAM, means even that time also I am running from RAM only , I am unable to find the solution. Please help me